Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for an H361DSWA, Series E2 (may be shown as E02)?
Issue:
Repair parts list for H361DSWA, series E2

Product Line:
Safety Switches

Resolution:
The repair parts for the H361DSWA, series E2 (E02) are as follows. No other parts are available.
-Line Base Assembly - 4051249250 (insulator, arc suppressor not included)
-Load Base Assembly - 4051250150
-Line and Load Base Mounting Screw - 4020506501 (3 for line & 2 for load)
-Insulator - 4052011401
-Arc Suppressor Assembly - 4051239950 (includes mounting screws)
-Lug Assembly - CL0306F (includes 6 lugs)
-Lug Assembly Mounting Hardware - 2342501700
-Receptacle - WRDK3034
-Receptacle Mounting Screws - 4510280101 (4 required)
-Handle Knob Kit - 4028344050K

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings