Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for the H362WC, series F4 (may be shown as F04)?
Issue:
What are the replacement parts for the H362WC, series F4?

Product Line:
Safety Switch

Environment:
Heavy Duty Safety Switch

Resolution:
The repair parts for the H362WC, series F4 (F04) are as follows. No other parts are available.
  • Line Base Assembly - 4056720750 (1 required; arc suppressor assembly not included)
  • Load Base Assembly - 4056604050 (1 required)
  • Line and Load Base Mounting Screw - 4020515101 (3 for line and 2 for load)
  • Arc Suppressor Assembly - 4056635550 (1 required)
  • Arc Suppressor Mounting Screw - 4020514501
  • Handle/Mechanism kit - HMR0306FN1 (includes handle, mechanism, rod, and lockplate)
  • Lug Kit - AL0306F (includes all line and load lugs)
  • Receptacle - 2541002311
  • Receptacle Mounting Screws - 4510280101 (4 required)

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings