Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for the H363AWC, series F5 (may be shown as F05)?
Issue:
Repair parts list for H363AWC, series F5

Product Line:
Safety Switches

Resolution:
The repair parts for the H363AWC, series F5 (F05) are as follows. No other parts are available.
-Line Base Assembly - 4056614250 (1 required; arc suppressor assembly not included)
-Load Base Assembly - 4056614550 (1 required)
-Line and Load Base Mounting Screw - 4020515101 (3 for line & 2 for load)
-Arc Suppressor Assembly - 4056635550 (1 required) (obsolete, no longer available, replaced by NNZ51874)
-Arc Suppressor Mounting Screw - 4020514501
-Handle/Mechanism kit - HMR10FN12 (includes handle, mechanism, rod, and lockplate)
-Lug Kit - CL10F (includes all line and load lugs)
-Receptacle - 2541002295
-Receptacle Mounting Screws - 4510280101 (4 required)

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings