Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for the HU362AWC, Series F5 (may be shown as F05)?
Issue:
Current Design Repair parts

Product Line:
Heavy Duty Safety Switch

Resolution:
The repair parts for the HU362AWC, series F5 (F05) are as follows. No other parts are available.
-Line Base Assembly - 4056612850 (1 required; arc suppressor assembly not included)
-Line Base Mounting Screw - 4020515101 (3 required)
-Arc Suppressor Assembly - 4056635550 (1 required)
-Arc Suppressor Mounting Screw - 4020514501
-Handle/Mechanism kit - HMR0306FN12 (includes handle, mechanism, rod, and lockplate)
-Lug Kit - CL0306F (includes all line and load lugs)
-Receptacle - 2541002311
-Receptacle Mounting Screws - 4510280101 (4 required)

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings