Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the difference between a bendable and non bendable 9007 lever arms, 9007HA1, HA2.
The bendable type is two pieces of flat steel, overlapping and secured in position by a screw. That screw can be loosened to allow the two pieces of the lever arm to forn an angle with each other. Tightening the screw then secures the lever in an angled position (i.e. dog-leg). The non bendable is either stamped steel or a casting which is fixed in position at manufacture and cannot be adjusted in the field.


CTA-ID : 14324

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings