Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Does SquareD/Schneider Electric offer a Non-Ventilated Transformer that is UL rated?
Issue:
Non Ventilated Transformers

Product Line:
LV Transformers

Environment:
Applies to LV Transformers by SquareD/Schneider Electric

Cause:
UL Ratings for Transformers

Resolution:

Yes and No,
Yes -- for Encapsulated Transformers up to 30kVA three phase and 25 KVA single phase
No -- for Non-Ventilated versions of Ventilated style units. It is not possible to keep the wiring compartment temperature at only a 5 Degrees C rise above a maximum ambient of 40 Degrees C as required for UL. SquareD/Schneider Electric recommends installers use a higher temperature rated cable (above 90?C) when terminating conductors in this style of Non-Ventilated Transformer.


Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings