Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Looking for the following replacement parts for 9001SKR1RH5: ring nut, locking thrust washer, trim washer, and compensating gaskets.
Issue:
9001SKR1RH5 Breakdown

Product Line:
Push Buttons and Operator Interface

Environment:
Harmony 30 mm 9001 SK Plastic Push Buttons

Resolution:
9001SK41 is ring nut; 6512240601 is SK locking thrust washer, trim washer is `nylon spacer` 6509705001, and 6509702001 is black compensating gasket.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings