Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What tenant circuit breakers can be used with ALL the EZM, 1 phase IN - 1 phase OUT, 125 A branch device meter sockets?
Issue:
Product Features

Product Line:
EZM Metering

Resolution:
ALL the EZM 1 phase IN - 1 phase OUT, 125 A branch device meter sockets use the QO, QO-VH, or QOH, 125 A max tenant circuit breakers. Example catalog number for 125 A - QO2125, QO2125VH, or QOH2125.

NOTE: There is no minimum ampere rating of a 2-pole tenant circuit breaker that can be used, there is only the 125 A maximum. QO-GFI and QO-EPD breakers may also be used on the EZM branch, taking into account the AIR limitation of the QO-GFI/EPD breakers.

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings