Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What tenant circuit breakers can be used with ALL the EZM, 3 phase IN - 1 phase OUT, 125 A branch device meter sockets?
Issue:
Product Features

Product Line:
EZM Metering

Resolution:

ALL the EZM 3 phase IN - 1 phase OUT, 125 A branch device meter sockets use the QO, QO-VH, or QOH, 125 A max tenant circuit breakers. Example catalog number for 125 ampere - QO2125, QO2125VH, or QOH2125.

NOTE: There is no minimum ampere rating of a 2-pole tenant circuit breaker that can be used, there is only the 125 A maximum.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings