Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is included with the MMLK500 lug kit?
Issue:
Product Design Features

Product Line:
Meter Pak and EZ Metering

Resolution:
This lug kit includes three double barrel lugs (for both phases and neutral). Each lug will accept (2) #3/0 - 500 kcmil conductors.

NOTE: This lug kit is designed ONLY to be used in the appropriate Meter Pak and EZM main devices.

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings