Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What tenant circuit breakers were used with the older 200 A single phase (IN & OUT), EZM branch devices (e.g. EZM112200 or EZM313200)?
Issue:
Product Design Features

Product Line:
EZM Metering Equipment

Resolution:
All the older 200 A, EZM branch device catalog numbers that were single phase (IN & OUT), but of the current main bus design (e.g. EZM112200 or EZM313200), used the old Q2M, Q2M-VH, or Q2MH, 100 - 200 A tenant circuit breakers. The Q2M type have been replaced with the PowerPacT Q frame, which has the same footprint and can be used in these 200 A, EZM branch devices.

NOTE: For 40 - 125 A applications, the old Q2M (or the new PowerPacT Q frame) can be substituted by using the EZM125QOA adapter kit with a QO, QO-VH, or QOH tenant circuit breaker.

Schneider Electric USA

Explore more
Category:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Category:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings