Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is included in the MMSK2 lug landing kit?
Issue:
Product design features

Product Line:
EZM and Meter-Pak metering equipment

Resolution:
The MMSK2 consists of three bus bar lug landing pads (for both phases and neutral). Each lug landing pad is supplied with two 1/2-13 studs on 1-3/4" centers and mounting hardware. One kit required per Meter-Pak device, order lugs separately.

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings