Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the handle padlock attachment for the 2 pole and 3 pole LA, LH, Q4, MA, and MH breakers?
Issue:
Lockout or Padlock Attachment for Legacy Breakers

Product Line:
Legacy Molded Case Circuit Breakers

Resolution:
The handle padlock attachment for 2 pole and 3 pole LA, LH, Q4, MA, and MH breakers is the HPALM. It locks the breaker in ON and OFF position.
Note: MA and MH circuit breakers will not lock in the ON position.

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings