Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the replacement overload relay part number for 8536SDO starter?
Issue:
8536SDO replacement overload relay

Product Line:
NEMA and Definite Purpose Contactors and Starters

Environment:
Type S Contactors and Starters

Resolution:
The replacement overload relay depends upon the device used and any Forms originally ordered. The following outlines the replacement parts:

Two pole starter with melting alloy (no overload form), 9065SDO7. (Discontinued)
Three pole starter with melting alloy (no overload form), 9065SDO8.
Starters with overload relay Form B, 9065SDO9B. (Discontinued)
Starters with overload relay Form B1, 9065SDO8B1. (Discontinued)
Starters with overload relay Form B2, 9065SDO9B2. (Discontinued)
Starters with overload relay Form H10, 9065SR210. (Discontinued)
Starters with overload relay Form H20, 9065SR220. (Discontinued)
Starters with overload relay Form H30, 9065ST220

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings