Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for a H326NR, series E1, E4, and E5 heavy duty safety switch?
Issue:
Repair parts

Product Line:
Heavy Duty Safety Switch

Resolution:
The parts listed here are the only field replaceable parts.
Complete interior - HN326NE1 (includes line & load base assembly, neutral assembly, arc suppressor assembly, box insulator, line phase insulators, and mounting hardware)
Line base assembly - 4055218550SEL (3 required and arc suppressor assembly is not included)
Load base assembly - 4055218750SEL (3 required)
Arc suppressor assembly - 4051204501 (3 required)
Lug assembly - 4405044601 (2 required per base assembly)
Neutral assembly - H600SN
Line base phase insulator - 4051201401 (2 required)
Load base phase insulator - 4055219101 (2 required)
Line & load base mounting screws - 4020600901 (2 required per base assembly)
Handle assembly - 4051217250SEL
Door thumb retainer - 4405049001
Door thumb screw - 4405043401
Handle knob kit (black & red knob at end of handle) - Series E1 is 4401142750, Series E4 and E5 is 4028343550
Neutral bonding strap - 4028300750SEL
Cross Arm Insulator – Consists of 4 parts: (2) 4055217701 (left and right side pieces); (1) 4055217801 (center piece); (1) 4055215701 (dust shield – retain the insulators by tying them together behind the cross arm)

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings