Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Do double throw safety switches have a center OFF position?
Issue:
What are the operational positions of a Double Throw Safety Switch?

Product Line:
Safety Switches

Resolution:
Yes, there is a center OFF position. There are three operational positions: ON - OFF - ON.  The ON - OFF - ON markings are located on the device nameplate or embossed into the front cover.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings