Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the part number for the internal auxiliary contact on NEMA devices?
Issue:
Internal auxiliary contact used on NEMA Contactors Sizes 00-2

Product Line:
NEMA and Definite Purpose Contactors and Starters

Environment:
Type S NEMA Contactors

Resolution:
Normally open is 9999SX11 and normally closed is 9999SX12. Please note these contacts are for use with NEMA devices up through size 2 only.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings