Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What lugs are provided and used with the EZM3400CBU?
Issue:
Product Design Features

Product Line:
EZM Metering

Resolution:
The EZM3400CBU is not provided with line side lugs from the factory. The suffix U of the catalog number indicates that the device meets EUSERC standards. EUSERC requires factory supplied lug landing pads to accept field installed lugs. In EUSERC locations, the lugs will normally be supplied by the utility company. For contractor supplied lugs, the lugs should be ordered separately. Lugs listed for use on this device will be noted on the devices wiring diagram (located inside the front cover). You may also refer to the attached drawing for a list of acceptable lugs.

Schneider Electric USA

Attachment(s)
EZM3400CBU dwg #3150.pdf [138.98 KB]
Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings