Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the size of the float on the 9049A60?
Issue:
Identifying float details for the 9049A60 kit

Product Line:
Pressure, Vacuum and Float Switches

Environment:
9049 Accessories for Float Switches

Resolution:
The height is 5.24" & the center (maximum) diameter is 4.2"


Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings