Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the standard lug kit for MH and MA breakers?
Issue:
What lug kit comes installed on the MA, MAL, MH and MHL circuit breakers?

Product line:
Molded case circuit breakers

Resolution:
The standard lug kit for the 300 - 1000 A breakers is AL900MA. The standard lug kit for the 1200 A is AL1000MA.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings