Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Do we offer strip heater options to prevent moisture condensation on Low Voltage Dry Type Distribution Transfomers when they are stored or intended to be operated intermittently?
Issue:
Strip heaters on Transformers

Product Line:
LV Transformers

Environment:
Applies to Low Voltage Transformers by SquareD/Schneider Electric

Cause:
Condensation may form and corrode Transformer elements

Resolution:

Supplemental heat, of which strip heaters is one form, is not offered as an option on SquareD/Schneider Electric  Low Voltage Dry Type Distribution Transformers. Should the application require supplemental heat, it is up to the installer to provide the necessary provisions.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings