Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Can you change the phasing on an EZM branch device?
Issue:
Is it possible to do phase balancing with EZM branch devices?

Product Line:
Metering

Resolution:
Yes, This available in 3 phase in 1 phase out branch units. there is a Z connector used to connect the line side power to the meter. These connectors can be rearranged for phase balancing in the field.



Schneider Electric USA

Explore more
Category:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Category:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings