Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Is a NEMA KS1 safety switch available?
Issue:
What is NEMA KS1 as it refers to enclosure types?

Product Line:
Safety Switch

Resolution:
All safety switches fall under NEMA KS1.

NEMA KS1 is in reference to the NEMA standard that addresses the manufacturing of safety switches. It is not an enclosure type, although enclosure types are addressed within the KS1 standard. Square D safety switches are manufactured to standards outlined in NEMA KS1 and UL98.

Schneider Electric USA

Explore more
Category:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Category:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings