Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
How does one get ground fault protection for an FA, FH, or FC I-Line style circuit breaker?
Issue:
How is ground fault protection achieved on an F-frame I-line breaker?

Product Line:
Molded Case Circuit Breakers

Resolution:
The ground fault module for an FA, FH, or FC frame circuit breaker is a GFM100FA. The breaker itself must have suffix G for a 24 V ground fault shunt trip accessory, which is factory installed only. It is important to know if there is sufficient room to install the module in the panel. The breaker and GFM module combined require the same space as an LA branch breaker and can only be mounted on the "wide" side of an HCP, HCW, HCWM, or HCRU panel.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings