Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the catalog number and description for a hookstick used on busway plug-in devices?
Issue:
What is the part number for the busway hooksticks?

Product Line:
I-Line busway and accessories

Environment:
Maintenance

Resolution:
The hooksticks are made of fiberglass and come in two sizes. Part number 515608 is 8 feet long and 515614 is 14 feet long.


Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings