Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the conductor temperature rating for the lugs of ALL the EZM main devices (main breaker, main switch, and main lug)?
Issue:
Application

Product Line:
EZM

Resolution:
The UL standards only test using 75 degree C conductors, so even though it might be marked on the lug itself stating '90 degree C', the devices are all UL tested and listed for use with 75 degree C conductors.
NOTE: 90 degree C conductors may be used if installed in accordance with the NEC (National Electrical Code) following the 75 degree C table.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings