Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the maximum temperature that a Mini Power-Zone enclosure surface can reach?
The maximum allowable surface temperature rise above ambient for a Mini Power-Zone (MPZ) is a 65degC.  With maximum ambient temperature of 40degC, the surface of the MPZ could reach 105degC (221degF.)  Remember the 24 hour average ambient should not exceed 30degC (86degF.)


CTA-ID : 2003059

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings