Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the available field installable undervoltage trips for PA/PH/PC circuit breakers?
Issue:
Is there a field installable undervoltage trip for PA1600 circuit breaker?

Product line:
Molded case circuit breakers

Resolution:
If the breaker is series 4 or higher, it will have accessory ports on the side and a field installable UVR may be added. Only the PA11121 and PA11124 (120 Vac and 240 Vac, respectively) undervoltage releases are available field installable.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings