Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the replacement for a QMB303T switch ?
Issue:
Cross Reference

Product Line:
QMB Switch

Cause:
Cross Reference

Resolution:
The QMB303T is an obsolete design 240V, Series 4 switch which utilized 3" of mounting space. The current replacement is a QMB321T (Series D2) switch which requires 4.5" of mounting space. The QMB306LEX extension kit will be required to install the QMB321T in a QW (38" wide enclosure) type interior manufactured before October 1984 but after 1961. An extension kit is not required to install the QMB321T in a QM type interior manufactured after 1961 but before October 1984.
NOTE: The QMB321T cannot be installed in QM interiors manufactured BEFORE 1961 or in the current Series E1 interiors.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings