Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Are standard sealing rings supplied with ALL the Ring Type MP Meter-Pak and EZM metering devices?
Issue:
Product Design

Product Line:
Meter Pak metering

Environment:
Meter Ring

Cause:
Supplied components

Resolution:
Yes. Standard Snap type aluminum sealing rings are supplied for each meter socket location on the MP Meter Pak and EZM branch devices.
NOTE: Screw type aluminum (29008W) and Snap type stainless steel (ARP00026) sealing rings are also available for field installation.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings