Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the conductor temperature rating for the lugs of an EZM main lugs terminal box device?
Issue:
Product Design Features

Product Line:
EZM Metering

Resolution:
The lugs are suitable for 75 degree C conductors. 90 degree C conductors may be used if installed in accordance with the NEC (National Electrical Code) Article 110.14(1)(b)(2) using the 75 deg C table.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings