Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What type of hub is available for use on the EZM main circuit breaker, main fusible switch, or main lugs terminal boxes?
Issue:
Product design features

Product Line:
EZM Metering equipment

Resolution:
For OUTDOOR applications, for conduit entry above live parts, use UL Listed raintight or liquidtight hubs. In an outdoor application, for conduit entry below live parts, or in an indoor application, use acceptable practices as allowed or dictated by the NEC (National Electrical Code), local codes, or utility company requirements.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings