Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Are the field installed electrical interlock kits also available factory installed on heavy duty safety switches?

Article available in these languages: Spanish

Issue:
Selection

Product Line:
HD SS

Resolution:
The electrical interlock kits can be provided factory installed in the NEMA 12 and 4X enclosures. It requires the use of the Product Selector for factory installation. The NEMA 1 or 3R Enclosures are NOT available with factory installed electrical interlocks.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings