Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Can you add auxiliary contacts to the LR9F overload relays?
Issue:
Do LR9F overload relays come with auxiliary contacts? Can extra be added in the field?

Product Line:
IEC Contactors and overload relays

Environment:
Tesys F overload relays

Resolution:
No, these overloads are provided with (1) normally open and (1) normally closed isolated contacts as standard.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings