Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
How may I install more than four 80 – 100 A branch circuit breakers in a NQ Panelboard?
Issue:
Installation of more than four 80-100A branch breakers in a NQ Panelboard.

Product Line:
NQ Panelboard

Environment:
Application

Resolution:
Up to four #14 - 2/0 AWG terminals are available in 400 A and 600 A NQ panelboard neutral assemblies. If additional neutral terminals are required for 80 – 100 A branch circuit breakers, NQ100AN neutral lugs may be added.  Each NQ100AN provides one #14 - 2/0 AWG terminal and requires two of the #14 - #4 AWG terminals in the neutral assembly.
If neutral terminations are not required for 80 – 100 A branch circuit breakers, simply uncheck the Neutral Load Connection Req’d box in the More Options field of the branch circuit breaker selection portion of the MAINS/FEEDERS screen in the Panelboard Product Selector in SE Advantage.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings