Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
You are currently viewing the content available in Vietnam. If you are looking for information for another region, please select the correct country from the top-left dropdown in the page and 'Navigate to Browse FAQs' in the Support menu.
How to connect the 4 Pole RCCB in 240V AC Single phase network.

⚠ CAUTION ⚠

The information provided in this FAQ being considered as confidential content, as it can be exclusively used internally.

This flag has been added automatically when the article is published with internal visibility only.

To use the 4 Pole RCCB in 240V AC single phase network, Pls check the wiring for test button on the top RCCB and follow that schematic
Confirm the functionality of the RCCB with the help of the Test Push Button. The RCCB should trip when the Test Push Button is pressed.

Schneider Electric Vietnam

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product: