Issue
Latest version of ION Setup software Installer is required.
Product Line
ION Setup 3.x.x
Environment
Software Installation Files
Resolution
The latest version can be downloaded using the link below:
ION Setup Software
The ION Setup Software, User Guide, and Device Configuration Guide can also be obtained by visiting link below
(Note: The latest version of ION Setup software may not be up-to-date from the link below):
ION Setup Software and Documents
ION Setup is only supported on Windows Vista and newer.1
Note that for the best compatibility, we strongly recommend that users run ION Setup on windows versions that are officially supported by Microsoft.
Kindly refer to the Microsoft link below for end of support information:
https://support.microsoft.com/en-us/lifecycle/search
Released for:Schneider Electric Global