Issue
Open Modsoft project with ProWORX 32
Product Line
ProWORX 32
Resolution
Yes. Programs created with Modsoft can be imported, then opened, using ProWORX 32 software. With the ProWORX 32 software up and running, go to <FILE> then <IMPORT DATABASE>, select File Type as (*.CFG) for Modsoft, then go into the folder that has the Modsoft *.CFG file and select it, click on the <OPEN> button and the conversion process will begin.
Open Modsoft project with ProWORX 32
Product Line
ProWORX 32
Resolution
Yes. Programs created with Modsoft can be imported, then opened, using ProWORX 32 software. With the ProWORX 32 software up and running, go to <FILE> then <IMPORT DATABASE>, select File Type as (*.CFG) for Modsoft, then go into the folder that has the Modsoft *.CFG file and select it, click on the <OPEN> button and the conversion process will begin.
Released for:Schneider Electric Global