undefined undefined
{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What is the part number for the Controller Inside Card for the ATV61/71 Drives?
Issue:
Part Number for the Controller Inside Card for the ATV61/71

Product Line:
Altivar 61, Altivar 71

Environment:
All serial numbers for ATV61/71

Cause:
N/A

Resolution:
The part number is VW3A3501. See attachment for a picture of the Controller Inside Card. This is a blank, programmable card. It does not come pre-programmed.

Schneider Electric Global

Attachment(s)
Controller Inside card.png [235.19 KB]
Explore more
Range:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: