Issue
What are the default report templates in PME 2020?
Product Line
Power Monitoring Expert 8.2 Standard Edition
Power Monitoring Expert 9.0
Power Monitoring Expert 2020
Environment
PME Web Application
Cause
To determine when a license is required to run a report
Resolution
1. The following are the default report groups that don't require a license:
PME 8.2, PME 9.0 and PME 2020
- Energy Management
- General
- Power Quality
- Usage Trending
2. The availability of these report groups is subject to licensing:
PME 8.2
- Billing and Allocation
- Energy Analysis
- Equipment Performance
- Generator Performance
- Power Capacity
- Power Efficiency
- UPS Performance
PME 9.0
- Backup Power Management
- Billing and Allocation
- Billing and Allocation / IT Billing
- Breaker Performance
- Capacity Management
- Energy Analysis
- Energy Analysis / Energy Modeling
- Insulation Monitoring
- Power Quality Performance
PME 2020
- Backup Power
- Billing
- Breaker Performance
- Energy Analysis
- Insulation Monitoring
- IT Billing
- Power Capacity
Note: Contact a Schneider Electric representative for more information about acquiring a license.
Released for:Schneider Electric Global