{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Is it possible to synchronize ATV process time with time server and get time according to local time zone?

Yes, since firmware version 2.1 on ATV600 and since firmware version 1.7 on ATV900, the time server function (SNTP) allows to get time with respect to time zone. Even switching between winder and summer time is possible.
Older fw versions allowed only to get UTC time.
It is recommended to configure SNTP via web server that allows more features than configuration by SOmove.
Printscreen in attachment shows example using a time server that is permanently running in schneider network (10.218.104.87) and with central european time zone including switching to summer time (DST enabled) based on start-end date and time.

Schneider Electric Global

Attachment(s)
timeZOne_SNTP.jpg [131.39 KB]
Explore more
Range:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: