undefined [object Object]
{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
How can your wire up an HOA on a ATV212 drive?
Issue:
HOA wiring and programming for ATV212 drives.

Product Line:
ATV212

Environment:
All

Cause:
programming and wiring HOA switch

Resolution:

RES is wired for HOA and (HO) is low and (A) is high

POT is wired to VIB PP and CC
4-20ma is wired to VIA and CC

FNOD-2 VIB or POT
F207= VIA or 4-20mA signal
F113 - RES program = 38 for auto manual.

Schneider Electric Global

Explore more
Range:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: