Microgrids explained

What is a microgrid?
A microgrid is a self-contained electrical network that can operate either connected to the utility grid or in an independent “island” mode. This capability allows you to generate your own electricity on-site and use it as needed. By incorporating distributed energy resources (DER), a microgrid can help save on energy costs by sending excess electricity back to the grid during peak demand. This not only improves reliability but also optimizes energy management.

How do microgrids work?
Microgrids utilize battery systems to store electricity generated on-site, offering a more efficient alternative to traditional power systems. They can deliver stored electricity during outages or when demand on the grid surges. These microgrids typically combine backup diesel generators with renewable energy sources, such as solar panels.

Who benefits from a microgrid?
Microgrids can now be used in remote areas with limited or no energy access. Various organizations, including municipal governments, airports, military bases, nature preserves, and vertical farms, can benefit from microgrids.

What does a microgrid cost?
The cost of microgrids varies based on their complexity and size. Microgrids operate under both the OpEx model in the EaaS framework and the CapEx model, depending on applicable local government policies.
Explore our software, services, and products for Microgrids
See how our customers benefit from Microgrids
Explore our latest insights on Microgrids
You might also be interested in:
1. Microgrid solutions from Schneider Electric
Schneider Electric offers efficient microgrid solutions based on a combination of Edge Control Systems, Connected Products, Applications, Analytics, and Services. Connected Products include Uninterruptible Power Supply (UPS), Grid-Tie String Inverters, and Hybrid Inverters. Applications, Analytics, and Services include EcoStruxure Microgrid Advisor and EcoStruxure Microgrid Operation, and Edge Control includes Harmony ST6 and EcoStruxure EV Charging Expert. We offer repeatable, scalable, and IoT-enabled microgrid solutions and end-to-end services, including electrical distribution services.
2. Different types of microgrids
Broadly speaking, there are three types of microgrids:
- Remote microgrids: These are also called off-grid microgrids. Remote microgrids can operate in island mode and be physically isolated from the utility grid in case of a lack of affordable and available transmissions or distribution infrastructure in the nearby area.
- Grid-connected microgrids: They have a physical connection to the utility grid through a switching mechanism at the point of common coupling (PCC); however, they can be disconnected into island mode and reconnected back to the main grid when required.
- Networked microgrids: These systems are also called nested microgrids and consist of several microgrids and separate DERs connected to the same utility grid circuit segment. They serve a wide geographic area.
3. Differences between a microgrid and a smart grid
Microgrids are different from smart grids. A microgrid is a self-sufficient and localized energy system serving a discrete geographic footprint, which may be a business center, hospital complex, etc. It includes distributed energy sources and multiple loads, which can be operated parallelly with the broader utility grid. Smart grids, on the other hand, are electrical grids that operate on a larger scale and can regulate energy flows from generation points to consumption points. They include communication, automation, and IT systems.
4. Designing of a microgrid
Schneider Electric offers a ready-to-use solution to help you design a microgrid, regardless of the application. Our pre-engineered microgrid control centers have all the components you need for power management, control, energy metering, and power monitoring. In addition, our microgrid management software – EcoStruxure – offers pre-engineered algorithms to make the functions standardized and reliable.
Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales inquiry online and an expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Center
Find support resources for all your needs, in one place.
的分散化和脱碳化,以及整个电网的数字化。由于电力是非常合理和可持续的解决方案,因此世界正变得越来越电气化。面向电力和电网的EcoStruxure,通过提供更绿色的发电、建立更好的电网、为消费者提供经济实惠的新能源,同时提高其盈利能力,帮助电力公司构建可持续的未来。