Search FAQs
Does Easergy T300 supports VPN connection using TLS security protocol or IPsec protocol?
Issue:
Customer wants To know if Easergy T300 supports VPN connection and with which security protocol(TLS or IPsec)
Environment:
Easergy T300
Resolution:
Easergy T300 supports VPN connection using TLS security, with the Router function enabled. IPsec is not available now.
Customer wants To know if Easergy T300 supports VPN connection and with which security protocol(TLS or IPsec)
Environment:
Easergy T300
Resolution:
Easergy T300 supports VPN connection using TLS security, with the Router function enabled. IPsec is not available now.
The standards applicable are listed below:
- User identification and authentication according to IEC62351-8.
- User's interface certificate management according to IEC62351-8.
- Communication Authentication according to IEC62351-5 when using DNP-3 and IEC60870-5-104 protocols.
Released for:Schneider Electric South Africa
Explore more
Range:
Explore more
Range: