Nossas Marcas

Bem-vindo ao website da Schneider Electric

Bem-vindo ao nosso site.
		
Como podemos ajudar você hoje?
Video: eConversion Live from the Lab 2: Mains Outage
eConversion is a patented high-efficiency mode for Schneider Electric Galaxy V Series (VS, VM, VL, VX) UPS that combines the best efficiency (up to 99%) with maximum load protection (IEC62040-3 class 1, VFI1.1.1 – equivalent to Double Conversion).
eConversion typically provides a 3x reduction of the UPS electricity consumption. This live video from the lab shows the system behavior in case of a mains outage.
Discover more via eConversion Savings Calculator .