Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What classes of fuses do the DT321 and DT321RB safety switches accept?
Issue:
Fuse data

Product Line:
Safety switches

Resolution:
These switches accept class H or K fuses as standard. Options include class R fuses (field install class R fuse kit). With Class H or K fuses installed, the switches are UL listed for use on systems with up to 10,000 RMS symmetrical amperes available fault current. With class R fuses (and class R fuse kit installed), the switches are UL listed for use on systems with up to 200,000 RMS symmetrical amperes available fault current.
NOTE: DO NOT USE RENEWABLE LINK FUSES IN SQUARE D SAFETY SWITCHES. The use of renewable link fuses may adversely affect user safety, impair reliability, and will void the warranty.

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings