Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Are 9421 circuit breaker operating mechanisms CE marked?
Issue:
Checking if the 9421 circuit breaker operating mechanisms are CE marked.

Product Line:
9421 Operating Mechanisms

Environment:
Operating Mechanisms and Disconnect Switches

Resolution:
The Class 9421 circuit breaker operating mechanisms do not require the CE Mark as they are not stand alone products, but only turn the associated circuit breaker on and off. Therefore, it is the circuit breaker that requires the CE Mark and not the mechanism.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings