Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the Knob Part Number for the 9001KS and 9001SKS Selector Switches?
Issue:
9001KS / 9001SKS Selector switch needs replacement knob

Product Line:
Pushbuttons

Environment:
30 mm selector switches

Resolution:
The knobs are the same for the illuminated and non-illuminated operators; except for the black and orange knobs which are opaque and for use on non-illuminated operators only.
ColorStandard Gloved Hand Coin Operated
Amber 9001A89001A24
Black 9001B119001B259001B18
Blue 9001L89001L249001L16
Clear 9001C89001C249001C16
Green 9001G89001G249001G16
Orange 9001S119001S25
Red 9001R89001R249001R16
White 9001W89001W24
Yellow 9001Y89001Y249001Y16

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings