Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is a Lock Kit available to lock the door of the NEMA 1 Homeline load center covers?
Issue:
Product Design Feature

Product Line:
Homeline Load Centers

Resolution:
Yes, PK6FL Lock Kit is suitable for use on current design Series 'S', indoor, convertible mains, Homeline load centers. Design Series 1, 2 and 3 covers do not accept field installable lock kits. Outdoor Homeline load centers do not accept a lock kit. However, a padlock hasp is provided to allow the cover to be padlocked closed.

EXCEPTIONS: HOM24L70F, HOM24L70S, HOM612L100F, HOM612L100S and HOM48L125GC load centers` covers do not accept a lock kit. These load centers do not have a door in the cover.


Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings