Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Aside from catalog number 9001 SKYP20 (or 9001 SKYP40, 9001 SKYP60, 9001 SKYP80, or 9001 SKYP1000), what else is needed to order this pendant station?
Issue:
What else is needed to order pendant stations aside from part numbers 9001 SKYP20 (or 9001 SKYP40, 9001 SKYP60, 9001 SKYP80, or 9001 SKYP1000).

Product Line:
9001SK Pendant Stations

Environment:
Push Buttons and Operator Interface

Resolution:
In addition to the catalog number, which designates a factory assembled pendant station, the customer must select all of the component pushbuttons and legend plates (and any other required components). Once the bill of material has been completed, the customer fills out the 9001 SKYP Key Sheet, which shows the factory where each component will be used in the completed, assembled pendant station. The completed Key Sheet is faxed to the Customer Service Team when the order is placed.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings